Drive systems for power tools

Indispensable helpers.

As the power tool market expands, greater demands are being placed on electric drive systems. They need to be powerful, dynamic, light, and efficient. Drives from maxon are true powerhouses, which meet these expectations with an efficiency level of over 90% and excellent controllability. 

Technology

Exceeding the limits of the technology.

maxon drive systems are ideal for battery-powered electric tools and the driving force behind power tools in the packaging industry, agriculture, and automated assembly.

  • Outstanding power density, dynamics, and precision
  • Low weight
  • Efficiency level of over 90%
  • Compact size
  • Excellent controllability
  • Long service life

The right drive for every device.

To offer the right solution for every device, our product portfolio includes a variety of drive types. Quality and reliability have the highest priority. Expertise and proprietary know-how enable us to develop custom drive systems in an interdisciplinary environment. In particular our brushless motor series offers excellent dynamics, high power density, and long service life due to extremely low wear.

Our product recommendations.

Whether they are used in the electronics, construction, or automotive industry, electric screwdrivers are essential for the automation of screwing processes. Our high-precision and powerful drives enable accurate torque and angle measurements as well as high dynamics and power density within small sizes.

DCX26L_Standardflansch

DCX 26

 

  • ∅26 mm
  • up to 14'000 rpm
  • up to 60 mNm
DCX32L mit Standardflansch

DCX 32

 

  • ∅32 mm
  • up to 11'300 rpm
  • up to 128 mNm
ECX_Torque_22_XL

ECX 22 Torque

 

  • ∅22 mm
  • up to 16'000 rpm
  • up to 80 mNm

EC-4pole 22

 

  • ∅22 mm
  • up to 25'000 rpm
  • up to 54 mNm
EC4pole30_long_150W

EC-4pole 30

 

  • ∅30 mm
  • up to 25'000 rpm
  • up to 95 mNm

High-speed operation and strong performance: Brushless motor technology provides stapling tools with the speed needed to take carton stapling to a new level as well as an electronically controlled and reproducible strapping process.

ECi30

EC-i 30

 

  • ∅30 mm
  • up to 15'000 rpm
  • up to 110 mNm
ECi40_short_50W

EC-i 40

 

  • ∅40 mm
  • up to 15'000 rpm
  • up to 340 mNm

The automation of repetitive manual work in agricultural production improves efficiency. Mechatronic drive systems from maxon are used in numerous applications such as lopping shears or plant tying machines.

EC-4 pole 22

 

  • ∅22 mm
  • up to 25'000 rpm
  • up to 54 mNm
ECX_Torque_22_XL

ECX 22 Torque

 

  • ∅22 mm
  • up to 16'000 rpm
  • up to 80 mNm
ECi30

EC-i 30

 

  • ∅30 mm
  • up to 15'000 rpm
  • up to 110 mNm
ecmax_

EC-max 22

 

  • ∅22 mm
  • up to 18'000 rpm
  • up to 23 mNm
ec30

EC-max 30

 

  • Ø30 mm
  • up to 15'000 rpm
  • up to 64 mNm

Corporate Blog

Success stories

With its global presence and engineering and production capacities, maxon is not only a component supplier but also a development partner for complete drive systems. All around the world, our drive solutions provide power in battery staplers, plant tying machines, saws, nail guns, and pressing tools. 
Packaging_automation_drivetechmaxon Story

Challenges for the packaging industry

Under the pressure of environmental concerns, the packaging industry is reorganising. Changing lifestyles and rising raw materials prices have completed this movement. The stakes are high, given that this sector, dominated by food processing, is…
Learn more
Kota 33 1500x1000

Shrink wrap packaging system.

Industrial automation is becoming increasingly necessary for industries. The agri-food sector is one of the industries making this transition. A Turkish company designs machines to automate this industry, using systems driven by Varvel gear motors,…
Learn more
Template DriveTech Parvalux chocolatmaxon Story

Parvalux: highly valued by chocolatiers

The art of chocolate requires precision, patience, and discipline, and if there is one company that knows how to support the best chocolate artisans, it is Savy Goiseau. The leading manufacturer of chocolate equipment in France, Savy Goiseau has…
Learn more

Frequently asked questions

  • How can we find out which drive is the best fit for our application, for example brushed or brushless?

    Our experts assist in selecting the drive and review all options in order to find the best solution for your application. In general, brushless motors are increasingly used in power tools. They are low-wear and thus achieve a longer service life than brushed motors.

  • How does maxon ensure that the temperature of the motor housing does not get too hot to hold?

    In principle, the surface of a hand-held device should not exceed approximately 43 °C if continuously in direct contact with the hand. The following points must be observed to keep the motor temperature low:

    • If possible, oversize the motor so that the load is lower.    
    • Choose a brushless motor suitable for higher speeds (if the application demands speeds equal to or greater than approximately 15,000 rpm).  
    • If PWM control is used, make sure that the inductance is not too low.  
  • Which drive is the best fit for battery-powered devices to achieve the highest level of efficiency?

    maxon drives are highly efficient, which makes them the perfect choice for battery-powered devices. In order to achieve the optimal level of efficiency, it is important to select a winding which is the best fit for the available battery power and the application operating point. In our standard product portfolio, we offer multiple windings for each motor. However, it is also possible to consider a custom winding if this is a better fit for the application.

Contact

How can we help you?

Our industrial power tools experts will be happy to help you.