maxon Story

A wasp shows the way

主题

needle_Copyright_Imperial-Collegeneedle_Copyright_Imperial-College

What do wasps have to do with brain surgery?  At first glance, not a whole lot. However, one species serves as the model for an innovative brain surgery needle that is being developed by a team of researchers from England. 

needle_Copyright_Imperial-College
driven0216_Fokusgrafik_E
EC20_flat_3W_13cm9cm
GP22_AR_9_13cm9cm
EPOS2_24_2_380264_9_13cm9cm
needle_Copyright_Imperial-College
driven0216_Fokusgrafik_E

© 2016 Imperial College

1/5

In tumor treatment, neurosurgeons today use a thin, rigid needle to inject medication into the affected brain tissue. This carries a relatively high risk of injuring healthy tissue, because a rigid needle only allows the surgeon to enter a certain region of the brain, following a straight path. The ideal solution would be a flexible operating tool.

This is where the London Imperial College comes in. In recent years, a team led by Prof. Rodriguez y Baena worked on developing a flexible robotic needle capable of reaching the deeper regions of the brain, while simultaneously avoiding especially sensitive areas. The young researchers seek to imitate the special mechanism employed by female wood wasps that use their thin but very strong drill-like stings to lay eggs inside the wood of trees. 

Under the project name STING (Soft Tissue Intervention and Neurosurgical Guide), the scientists developed a prototype consisting of four segments with an overall diameter of 2.5 millimeters, hold together by a puzzle-like interlocking mechanism. maxon drives provide the back-and-forth motion of the segments.

“The whole range”

Dr. Secoli is a member of the Mechatronics in Medicine Lab at the Imperial College. He selected the brushless maxon EC20 flat motor with a GP22 planetary gearhead for the application. An EPOS 24/2 positioning controller provides exact positioning. “Easy access to the API (Application Programming Interface) was the major key criterion of selection. On top of that, for fast-prototype system, maxon is the only manufacturer that offers the whole range of products: motor, gearhead, controller” says Dr. Secoli.

In early 2016, the team received a grant of 8.3 million euros from the European Union within the funding scheme Horizon2020. The new project codename EDEN2020 (Enhanced Delivery Ecosystem for Neurosurgery www.eden2020.eu), aims to set a new standard in the field of neurosurgical diagnostics and therapy by 2020.

Author: Anja Schütz