maxon Story

Hair today, gone tomorrow.

Topics

Joe Before drivetechJoe Before drivetech

How maxon helped a Dublin clinic cope with the astonishing increase in hair transplants during the pandemic.

Since the start of the coronavirus pandemic, Ailesbury Hair Clinic, based in Dublin, Ireland, has seen a 50 per cent increase in people coming forward for hair replacement treatments. When the clinical couldn’t find a next level surgical tool to harvest hair follicles for treatments, it decided to design one for themselves and turned to precision drive and motor specialist, maxon for help.

Hair loss affects millions of men and women globally and many of these saw the chance to have treatment and recover while working from home as a convenient opportunity. Ailesbury Hair Clinic, which specialises in the minimally invasive aesthetic hair integration follicle unit extraction (AHI FUE) procedure and has won numerous awards for its advanced technique, saw a huge increase in demand for treatment.

Most existing follicle extraction devices are heavy and bulky, so the clinic’s experts decided to call on their 20 years industry experience to design a new device for themselves. Having been involved in developing various medical devices and surgical tools over the years, the clinic’s experts were confident they could design a more streamlined and effective hand-held follicle extraction device that was light, robust, fast and had wireless capabilities.

Ioannis Ypatidis, a programmer and roboticist, is the Project Manager who developed the new device. He chose maxon's products for the final design because of their small size and relatively high torque compared to similar options available from other manufacturers. After initially deciding to go with a geared motor for their device, the team contacted Martin Leahy, maxon's Sales Engineer in Ireland, to discuss concerns about noise and vibration.

Joe After Results drivetech

«The maxon motor within the tool is powerful and extremely efficient»

“Martin directed us towards choosing a direct drive motor without gears because this would eliminate the issues around noise and vibration while increasing the product's service life,” explained Ioannis. “His advice was extremely valuable and saved us a lot of time on this project.

“We were going in the wrong direction with our motor choice and consulting Martin allowed us to adapt without wasting a lot of unnecessary time and resources in testing the wrong solutions.”

The innovative new drill is exact, reliable and extremely small, the nose is just 0.8 mm. The motor is from maxon’s configurable DCX direct drive range which facilitates the handheld design by offering high power density and torque in a small design. Using a direct drive solution increased the device’s service life and offered a reduction in weight and vibration compared to geared motor solutions. Using a rechargeable battery system has made the new tool portable and transferable from clinic to clinic and country to country without considering different power supplies.

“People are more comfortable now with this type of hair restoration treatment. It is considered quite mainstream and is a fairly simple and acceptable procedure. Depending on how many hairs are grafted, it usually takes approximately 3 to 4 hours of treatment, with breaks. The maxon motor within the tool is powerful and extremely efficient, providing the user with better scope for precision, power and perfection in client results,” added Ioannis.

Ailesbury Hair Clinic specialises in treating men and women for hair loss and its minimally invasive AHI method has been used to treat thousands of people to an award-winning standard over its two decades in business. This meant that quality was the main consideration for its team on this project.

“We knew maxon’s motors were deployed on Mars on the Perseverance rover. We saw this as a huge validation of maxon’s quality and figured if it's good enough for Mars, it will be good enough for us,” concluded Ioannis.

Author: maxon HQ